BRAKE#.SAFE.SBT.STATE

Description

Read the state of the Safe Brake Test (SBT) on the specified brake. The return value is one of the following:

Value

Description

0

The brake is not tested.

1

The brake has been successfully tested.

2

The brake failed to test. It may be broken.

3

The brake is applying.

4

The brake is tested.

5

The brake is releasing.

Code

--> BRAKE1.SAFE.SBT.STATE
0

Context

For complete SBT information refer to SBT (Safe Brake Test).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-00-00-000

Implemented in SMM revision v0.32

General Information

Type

Read Only

Units

N/A

Range

0 - 7
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
BRAKE1.SAFE.SBT.STATE

40f3h

01h

Unsigned8

-

-

Read only

No

BRAKE2.SAFE.SBT.STATE

40f3h

02h

Unsigned8

-

-

Read only

No